Technical FAQs

Ask a Question

What is the minimum and maximum wire size that can be used in the screw terminal on the LC1K06/09/12 contactor?

Mimimum: One # 18 AWG
Maximum: One #12 AWG or two #14 AWG


CTA-ID : 2010954
Was this helpful?
What can we do to improve the information ?