Technical FAQs

Ask a Question

Can a power pole be added to an NEMA size 3, 4, 5, 6 or 7 contactor or starter?

A size 0 through 2, 30 amp and 60 amp, power pole can be added to these devices. A 9999 SBT1 adapter bracket is required.


CTA-ID : 2011322
Was this helpful?
What can we do to improve the information ?