Technical FAQs

Ask a Question

What is the magnetic trip setting for the LC I line breaker?

Product Line:
Legacy Circuit Breaker
LC Type

Environment:
Electrical Distribution Equipment

Resolution:
The magnetic trip setting for the LC breakers below:

3 Pole (3P) Devices:

LC36300 is 1500 low, 3200 High
LC36350 is 1750 low, 3200 High
LC36400 is 1500 low, 3200 High

LC36450 is 2250 low, 4200 High
LC36500 is 2500 low, 4200 High
LC36600 is 3000 low, 4200 High

2 Pole (2P) Devices:

LC26300 is 1500 low, 3200 High
LC26350 is 1750 low, 3200 High
LC26400 is 1500 low, 3200 High

LC26450 is 2250 low, 4200 High
LC26500 is 2500 low, 4200 High
LC26600 is 3000 low, 4200 High


CTA-ID : 2011882
Was this helpful?
What can we do to improve the information ?