Technical FAQs

Ask a Question

What is the maximum number of cover-mounted operators that can be installed in the NEMA size 00 through NEMA size 3 Class 8502 / 8536 contactors and starters using the standard NEMA 1 general purpose enclosure?

There are 2 rectangular knockouts provided. One for a pilot light and the other is for the rectangular push button or selector switch kit.

Note: This applies to the standard slip-on cover style enclosures and does not apply to devices supplied with oversized enclosures using hinged door.


CTA-ID : 2009822
Was this helpful?
What can we do to improve the information ?