Technical FAQs

Ask a Question

What is the ATV58 keypad part number?

Issue:
What is the ATV58 keypad part number?

Product Line:
All ATV58 drives

Environment:ALL ATV58 drives

Cause: ATV58 keypad part number Resolution:
Part number is VW3A58101U
This keypad part number is good for the entire range of ATV58 drives.
*** NOTE: The exception to this is for the ATV58HC19N4 size drive. As of January 2005, this size drive requires the VW3A58101V5337 keypad. ***
Both of these part numbers are now obsolete and no longer available.

Was this helpful?
What can we do to improve the information ?