Technical FAQs

Ask a Question

What type of fuse is required for the Class 9999 Type SF* and SFR* fuse holders?

Product Line:
 
Type S Style Accessories and Components

Resolution:
 The fuse type and ratings are as follows:

9999SF3 - Accepts one standard 600 volt 6 amp maximum Bussman Type KTK or equivalent fuse.

9999SF4 - Accepts two standard 600 volt 6 amp maximum Bussman Type KTK or equivalent fuse.

9999SFR3 - Accepts one standard 600 volt 6 amp maximum Bussman Type KTKR or equivalent fuse.

9999SFR4 - Accepts two standard 600 volt 6 amp maximum Bussman Type KTKR or equivalent fuse.


CTA-ID : 2011919
Was this helpful?
What can we do to improve the information ?