Technical FAQs

Ask a Question

What is the sealed and inrush VA of the LX1FG coils used in the LC1F185 & LC1F225 IEC contactors?

Product Line:

Tesys F line Contactors and Accessories
Inrush, 50Hz: 805 VA; 60 Hz: 970VA
Sealed 50Hz: 55 VA; 60Hz: 66 VA

CTA-ID : 2011803
Was this helpful?
What can we do to improve the information ?