Technical FAQs

Ask a Question

What is the difference between the LA36400 and LC36400 being used at 480 Vac?

Product Line:
Legacy Circuit Breakers
I Line

Electrical Distribution Equipment

The LA is rated at 480 v 30 KAIC and the LC at 480 v is 65 KAIC and also LA needs 6 inches of mounting space and LC needs 7.5 inches of mounting space.

CTA-ID : 2011632
Was this helpful?
What can we do to improve the information ?