Technical FAQs

Ask a Question

Catalog number for a replacement coil number 31071-754-50 is obsolete. Is there a replacement?

Replacement parts for 8501 and 8903 obsolete devices

Product Line:
8501 type H and 8903 type LL devices

Products sold and used in the United States

Obsolete replacement parts

These were the mechanical latch attachments for all the old Class 8501 Types H and Class 8903 Types L mechanically held machine tool relays and lighting contactors.
Where Used:
All Class 8501 Types HL & HML2, 3, 4, 6, 8 poles

All Class 8501 Types HXL & HXML8, 10, 12 poles
All Class 8903 Types LL2, 3, 4 poles
All Class 8903 Types LL6, 8, 10 poles

Parts Status:
Obsolete, complete device must be replaced.

CTA-ID : 2011521
Was this helpful?
What can we do to improve the information ?