Technical FAQs

Ask a Question

Can a customer order a class 2510 Nema Type 7&9 manual starter with 1 inch conduit openings?

No, the Nema type 7 & 9 enclosure only comes with 0.75 inch conduit openings.


CTA-ID : 2012068
Was this helpful?
What can we do to improve the information ?