Technical FAQs

Ask a Question

Does Square D offer a Nema 3R, 1200amp, 3-pole, non-fusible, Double throw safety switch, with a solid neutral?

Issue:
Product Design Features

Product Line:
Double Throw Safety Switches

Environment:
Ampere rating

Cause:
Application

Resolution:
Square D/SE does NOT offer any standard Double Throw Safety Switches rated at 1200amp, there are no Double throw switches over 600amp. 

NOTE: There are some Transfer Switches offered by Schneider Electric Field Services, West Chester. They are not UL Listed and a catalog number for a 1200amp is TSW36120 and the field installable solid neutral is N12.
PLEASE CONTACT Field Services with any questions.

 
Was this helpful?
What can we do to improve the information ?