Technical FAQs

Ask a Question

Can you get more than the standard four aux contacts on a Masterpact NT breaker?

Issue:
What is the maximum number of aux. contacts you can get on a Masterpact NT breaker?

Product Line:
Masterpact NT

Resolution:
  • The NT comes with four form C contacts, 4a4b.  There is no standard offer for adding more.
  • Additional OF contacts can be applied to the NT breaker (for a total of 12) by ordering from Services.  The plant supplies the parts and Services installs and tests and makes the sale to the customer. 
    The catalog number will have an "N" in position 19.
Was this helpful?
What can we do to improve the information ?