Technical FAQs

Ask a Question

Can you get the ATS48 softstart as just a chassis open style unit?

The units ATS48D17Y to C11Y are rated IP20
The units ATS48C14Y to M12Y are rated IP00

Therefore technically they are open style. You can not obtain these units without the plastic outer covering which is the question at hand.


CTA-ID : 2012478
Was this helpful?
What can we do to improve the information ?