Technical FAQs

Ask a Question

Can QO circuit breakers and surger arrestors be used in a Cutler-Hammer load center?

Issue:
Product application

Product Line:
QO Circuit Breakers

Environment:
Use in competitive panels

Cause:
Clarification

Resolution:
Square D QO breakers and surge arrestors should be used only ins Square D QO load centers and NQ panel boards.


CTA-ID : 2012706
Was this helpful?
What can we do to improve the information ?