Technical FAQs

Ask a Question

What is the dissipated power in watts for the ATS48D75Y soft starter for calculating heat loss for enclosure sizing?

The power dissipation in watts with the shorting / bypass contactor is 25W and without the shorting / bypass contactor is is 245W.

The the associated literature for additional details regarding mounting this product in an enclosure.

CTA-ID : 2012896
Was this helpful?
What can we do to improve the information ?