Technical FAQs

Ask a Question

With an Econoflex drive, why is it not possible to get the drive to Autotune?

It is possible to autotune this drive. If this unit has bypass, the isolation contactor must be closed to provide a good connection between the drive and the motor.

Also, there must not be a fast stop or freewheel stop active.

Make sure that any logic input programmed as Fast Stop or Free Wheel stop is on (high or with +24 VDC present), but all other logic inputs have to be off (low).
Was this helpful?
What can we do to improve the information ?