Technical FAQs

Ask a Question

Do we have a UL 489 listed 480 Vac M9?

The UL 489 version has a 240Vac rating (.5A-35A)
The UL 1077 listed M9 is rated for 480Y/277, not 480 delta.
The IEC version has a 440Vac rating

CTA-ID : 2013006
Was this helpful?
What can we do to improve the information ?