Technical FAQs

Ask a Question

What is the difference between the U-Line Starter Base and the Self-Protected Starter Base?

The Starter Base is a contactor and an overload relay only. The Self-Protected Starter Base is a circuit breaker disconnect with a contactor and an overload in one package.

CTA-ID : 2013061
Was this helpful?
What can we do to improve the information ?