Technical FAQs

Ask a Question

What is the terminal data for the NEMA size 3 contactors and starters?

Power terminals - one #14 to #1/0 AWG copper wire per phase; control terminals - two #16 - #12 AWG copper wire per terminal.


CTA-ID : 2013722
Was this helpful?
What can we do to improve the information ?