Technical FAQs

Ask a Question

What is the part number for the 7`` Enclosure Fan for the 8839?

Issue:
Part number for 7" stirring fan

Product Line:
Enclosed ATV66 driv

Environment:
All models

Cause:
None

Resolution:
2601631100 is the part number for the 7 inch stirring fan used in the enclosed ATV66 drives. It is operated by 120 VAC from the control transformer in the enclosure. This fan is not actually part of the ATV66 drive and should not be confused with the heatsink, capacitor bank and/or stirring fans that are on some of the ATV66 drives.

CTA-ID : 2013081
Was this helpful?
What can we do to improve the information ?