Technical FAQs

Ask a Question

When is it recommended to use the W816366180111 TeSys overload relay spacer?

Anytime the smaller OLR`s (LRD01 - LRD21 or LRD1508 - LRD1521) are direct mounted to the LC1D25 or LC1D32 contactors, utilizing the W816366180111 spacer provides good stability of the relay on the contactor, mainly while cabling.

CTA-ID : 2014473
Was this helpful?
What can we do to improve the information ?