Technical FAQs

Ask a Question

Do the 9998SL25 or 9998SL26 contact kits provide the springs?

No, springs are not included. The springs do not come in direct contact with the current flow and therefore should not need replacing. If the springs do need replacing chances are the mechanical life of the contactor has expired.

CTA-ID : 2013461
Was this helpful?
What can we do to improve the information ?