Technical FAQs

Ask a Question

On the 883958M is the line reactor installed before or after the Circuit Breaker?

It is installed after the Circuit Breaker. It is fed from the distribution block and the output of the line reactor is connected to the Line Contactor or the drive inputs.


CTA-ID : 2014284
Was this helpful?
What can we do to improve the information ?