Technical FAQs

Ask a Question

Can a LAL, LHL or Q4L circuit breaker be installed in a MA1000S, MA1000F and MA1000R circuit breaker enclosure?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Cause:
Application

Resolution:
Yes, the LAL, LHL or Q4L circuit breaker can be installed in the MA1000S, MA1000F or MA1000R. They could not be installed in the MA1000AWK nor MA1000DS enclosures.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. FOR A NEW INSTALLATION, CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 (800A max) OR P1200 (1200A max) SERIES OF ENCLOSURES.


CTA-ID : 2014554
Was this helpful?
What can we do to improve the information ?