Technical FAQs

Ask a Question

What type of fuses does a QMB322TW accept?

Issue:
Application

Product Line:
QMB

Cause:
Selection of fuse type

Resolution:
This QMB switch accepts Class H or Class K fuses as standard or Class R fuses with rejection kit QMB36R installed. Since this is a twin switch unit, two QMB36R kits would be needed.


CTA-ID : 2014596

Was this helpful?
What can we do to improve the information ?