Technical FAQs

Ask a Question

Do the LAD9 & LA9D 3-pole power connection kits consist of a set of two connections?

Issue: 
Do the LAD9 and LA9D kits include both line and load side connections? 

Product Line:
 Tesys D-line accessories

Environment:
Products sold and used in the United States
 
Cause:
 Identifying kit components
 
Resolution:
 
Yes, line and load side connections are included.


CTA-ID : 2013867
Was this helpful?
What can we do to improve the information ?