Technical FAQs

Ask a Question

Customer bought a 9001KM1. Now needs a two position illuminated selector switch with green knob.

The knob would be 9001G8 + 9001KS11. Remove the liner from the back. Will need to add contactor.

Not FAQ


CTA-ID : 2014371
Was this helpful?
What can we do to improve the information ?