Technical FAQs

Ask a Question

How many auxiliary contacts can be installed on a NEMA size 00 reversing contactor or starter?

Qty (2) are allowed for each contactor; however, they must all be installed on the outer side of the contactor, as the mechanical interlock between the contactors prevents any auxiliary contacts from being installed on the inner side.

CTA-ID : 2014169
Was this helpful?
What can we do to improve the information ?