Technical FAQs

Ask a Question

Can I get a red pilot light for an 8539 NEMA 7/9 combination starter?

Issue:
Can I get a red pilot light for an 8539 NEMA 7/9 combination starter?

Product Line:
Nema starters/contactors sold and supported in the USA.

Environment:
Replacement

Cause:
Maintenance

Resolution:
Yes. The part number is 2949520209.

Revison: Effective 2011, Nema 7 and 9 enclosures are no longer offered for our Nema starters/contactors. The 2949520209 is available for replacement purposes only. 


CTA-ID : 2014437
Was this helpful?
What can we do to improve the information ?