Technical FAQs

Ask a Question

What are the dimensions of a MA1200S circuit breaker enclosure?

Issue:
Product Features

Product Line:
Circuit Breaker Enclosure

Cause:
Dimensions

Resolution:
The MA1200S enclosure dimensions are 20.25" W x 51.8" H x 7.5: D. 
See attached MA1200S Drawing #3448
This link will also access the MA1200S drawing:
http://static.schneider-electric.us/docs/Circuit%20Protection/Circuit%20Breaker%20Enclosures/3448.pdf





CTA-ID : 2014677
Was this helpful?
What can we do to improve the information ?