Technical FAQs

Ask a Question

Can the trip unit be replaced on an SE circuit breaker?

Issue:
Can the trip unit be replaced on an SE circuit breaker?

Product Line:
SEF or SED

Environment:
Series B trip unit only.

Cause:

Resolution:
The SE breaker is the only Series B Micrologic breaker that can have the trip unit replaced in the field. Replacement must be done by Services.


CTA-ID : 2014209
Was this helpful?
What can we do to improve the information ?