Technical FAQs

Ask a Question

What document that shows the correct part numbers for the shorting contactor that is printed incorrect in the 30072-450-61 ALTISTART. 48 Y-Range Soft Start Controllers Installation Guide?

30072-450-87 ERRATA for bulletin 30072-450-61, ALTISTART. 48 Y-Range Soft Start Controllers Installation Guide.
This Errata contains other corrections as well. It should be included with all new ATS48 soft starters.


CTA-ID : 2014967
Was this helpful?
What can we do to improve the information ?