Technical FAQs

Ask a Question

Are any parts available for the 8660 AlphaPak starters?

Product Line: 8660 AlphaPak solid state reduced voltage starters


Environment: All Class 8660 AlphaPak starters


Cause: N/A


Resolution: The 8660 AlphaPak starters are obsolete. No parts are available for these. Replace with current ATS01, ATS22, or ATS48 softstarters.
Was this helpful?
What can we do to improve the information ?