Technical FAQs

Ask a Question

What is Form Y48 on the Class 8903 Type L lighting contactor?

Substitutes DC coil for AC coil,

Note this is a factory option only and is available only up through 7 poles. For use on electrically held devices only.

The following voltages are available, V code must be used in conjunction with Form Y48. For example, to obtain 4 pole open style electrically held device with 24 vdc control coil order 8903LO40V53Y48.

DC Voltage Code

24 V53Y48
32 V54Y48
48 V56Y48
115/125 V62Y48
230/250 V66Y48



CTA-ID : 2014638
Was this helpful?
What can we do to improve the information ?