Technical FAQs

Ask a Question

What is the current rating on the contacts of a 9038 switch?

The 9038 devices are Nema A600 control circuit rated, which does not allow direct motor control, requiring a contactor or starter. The motor horsepower ratings vary with single or three phase as well as voltage. See Digest 173, p 20-26.

CTA-ID : 2015380
Was this helpful?
What can we do to improve the information ?