Technical FAQs

Ask a Question

What is the Terminal Lug Data for a CH365DS, Series E2 Heavy Duty safety switch?

Issue:
Product Features

Product Line:
Safety Switches - Canada

Cause:
Clarification

Resolution:
The lugs on this device will accept (1) #1 AWG - 600 kcmil or (2) #1 AWG - 250 kcmil copper conductors per phase.


CTA-ID : 2035475
Was this helpful?
What can we do to improve the information ?