Technical FAQs

Ask a Question

What is the LHL3640030DC1616 breaker.

Product Line:
Legacy Circuit Breakers

Electrical Distribution Equipment

This is a LHL36400 that is rated for a 500VDC application and which has the combination accessories of the 24VDC shunt trip and the 1A/1B auxiliary interlocks.

CTA-ID : 2015597
Was this helpful?
What can we do to improve the information ?