Technical FAQs

Ask a Question

Which trip unit should be selected to get LSIG trip features on PowerPact P and R, and Masterpact NT and NW breakers?

Product Line:
Circuit Breakers
PowerPact P, and R
MasterPact NT and NW

Environment:
Electrical Distribution Equipment

Resolution:
The 6.0A, 6.0P, or 6.0H trip unit. Catalog numbers S144A, S164A, and S174A respectively.



For help with Micrologic trip units and modbus communications for Masterpact and Powerpact P and R circuit breakers, consult instruction manuals:
Powerpact P, R, and Masterpact NW, NT Micrologic™ types 2.0, 3.0 and 5.0 Trip Units, see 48049-207-05
Powerpact P, R, and Masterpact NW, NT Micrologic™ 2.0A, 3.0A, 5.0A, and 6.0A Trip Units, see 48049-136-05
Powerpact P, R, and Masterpact NW, NT Micrologic™ 5.0P and 6.0P Trip Units, see 48049-137-05
Powerpact P, R, and Masterpact NW, NT Micrologic™ 5.0H and 6.0H Trip Units, see 48049-330-03
 
Was this helpful?
What can we do to improve the information ?