Technical FAQs

Ask a Question

Customer is looking for a 8910DP42V09U2. What does U2 mean?

U2 is addition of CSA label to 8910DP42 contactors. Ratings on the device nameplate will change from 40 FLA and 50A Res. (600V Max) to 40 FLA and 50A Res. (277V) and 40A Res (480V & 600V).

CTA-ID : 2035339
Was this helpful?
What can we do to improve the information ?