Technical FAQs

Ask a Question

What is the replacement starter in an enclosed 2-pole NEMA size M-1 manual motor starter for AC applications?

To replace only the starter, use the 2510MCO1 for the ones with the square push button operators or 2510TCO1 for the ones with the toggle operator.


CTA-ID : 2015984
Was this helpful?
What can we do to improve the information ?