Technical FAQs

Ask a Question

What is the part number for the replacement bulb for the Pilot Light supplied in a size 1, NEMA 7/9 enclosed contactor or starter?

Since the cover-mounted units for the explosion proof starters are made by Curlee, the bulb would need to be obtained from them. The entire pilot light assembly can be purchased from Square D by ordering part number 29495-20209 but we cannot provide just the bulb.


CTA-ID : 2015609
Was this helpful?
What can we do to improve the information ?