Technical FAQs

Ask a Question

Are the QO Load centers, both single and three phase, supplied with a neutral assembly as standard?

Issue:
Product Design features

Product Line:
QO Load centers

Environment:
Main Neutral Assembly

Cause:
Voltage system applicaton

Resolution:
Yes, ALL the QO single and three phase load centers come standard with a neutral assembly for the voltage systems.


CTA-ID : 2015858
Was this helpful?
What can we do to improve the information ?