Technical FAQs

Ask a Question

Is there is any restriction on the mounting position of a 300A Type SX mechanically held lighting contactor?

The mechanically held devices can only be mounted upright, in the vertical plane, with L terminals at the top and T terminals at the bottom.

CTA-ID : 2015542
Was this helpful?
What can we do to improve the information ?