Technical FAQs

Ask a Question

Can a QO200 molded case switch be used in a QO load center?

Issue:
Product design features

Product Line:
Branches

Environment:
QO Load centers

Cause:
Application

Resolution:
Yes, but the Application must meet the NEC requirements.
Was this helpful?
What can we do to improve the information ?