Technical FAQs

Ask a Question

Customer has p/n 31071-754-51. What is the replacement for it?

These were the mechanical latch attachments for all the old Class 8501 Types H and Class 8903 Types L mechanically held machine tool relays and lighting contactors.
Where Used:
All Class 8501 Types HL & HML2, 3, 4, 6, 8 poles

All Class 8501 Types HXL & HXML8, 10, 12 poles
All Class 8903 Types LL2, 3, 4 poles
All Class 8903 Types LL6, 8, 10 poles

Part Status:
Obsolete, complete device must be replaced. Reference to CCR for replacement.

CTA-ID : 2015580
Was this helpful?
What can we do to improve the information ?