Technical FAQs

Ask a Question

Is the catalog number H368 CSA certified?

Issue:
Product design features

Product Line:
Heavy Duty Safety Switches

Environment:
Codes and standards listing

Cause:
Application

Resolution:
Yes. This switch is both UL listed and CSA certified.


CTA-ID : 2025185
Was this helpful?
What can we do to improve the information ?