Technical FAQs

Ask a Question

What is the neutral CT catalog number for a R frame Powerpact and Compact NS1600b - NS3200 breaker?

Product Line:
Powerpact R and Compact NS1600b-3200

Environment:
All series & versions

Resolution:
Neutral CT`s are as follows:
250A            S48916
400-1600      S34036
2000            S48896
2500-3200    S48182


CTA-ID : 2025220
Was this helpful?
What can we do to improve the information ?