Technical FAQs

Ask a Question

What type of fuses does a QMB323TW accept?

Issue:
Application

Product Line:
QMB

Cause:
Selection of fuse type

Resolution:
This QMB switch will accept Class H or Class K fuses as standard or Class R fuses with rejection kit QMB100R. Since this is a twin switch unit, two QMB100R would be required; one for each switch. 



Revised 3/22/04



CTA-ID : 2016717
Was this helpful?
What can we do to improve the information ?