Technical FAQs

Ask a Question

What is the difference between FA and FY I-Line breakers?

Product Line:
Legacy Circuit Breakers
I Line

Environment:
Electrical Distribution Equipment

Resolution:
FY breakers are available from 15-30 amp one pole only and the 15 and 20 amp versions are SWD (switch duty) rated. These are generally used for lighting loads in I-Line 277V applications.
FY breakers have a 14k AIC rating at 240v or 277v.
FA breakers are available from 15-100A, and have an 18k AIC rating at 240v or 480Y/277v, but are not SWD (switch duty) rated


CTA-ID : 2016727
Was this helpful?
What can we do to improve the information ?