Technical FAQs

Ask a Question

Are viewing windows offered on combination starters?

Form G36 is the addition of a viewing window to a NEMA Type 1, 3R, 4 (Stainless Steel Only), 12/3R combination starters. The window will be on the front and is large enough to observe the status/position of the disconnect switch blades. Applicable to Class 8538/8738 NEMA Size 0, 1, 2, 3 devices only.





CTA-ID : 2015589
Was this helpful?
What can we do to improve the information ?